Hello:
I have a issue when using the TPS61094, the SUP pin is connected to a supercapacitor, during the test I found that when the external power supply is disconnected, the supercapacitor enters the boost-on mode , but there is a level voltage on the VIN pin of the TPS61094, the voltage on the VIN pin is reduced to 0V until the supercapacitor discharge ends,What is the reason?
Input voltage:5V ;Target output voltage:3.8V