Hi Teams,
In WEBENCH@ POWER DESIGNER, I select TPS546D24A (stackable buck converter) in DC/DC Power Designs. The TPS546D24A can support up to stackable four phase operation and the output current is up to 160A. But the output current design is limited to 80A with stackable two phase operation. How can I use this tool to design output current up to 160A in TPS546D24A?