This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65950 not generating VMMC1

Other Parts Discussed in Thread: TPS65950, DM3730

Hi,

I have our custom board with DM3730 & TPS65950, i am not getting VMMC1 voltage on TPS65950 device.

I have checked the power up sequnce and all the voltages like VIO,VPLL1, VDD1, VDD2 are coming up correctly. It seems DM3730 is not sending I2C command to TPS device to switch on the VMMC1 volatage.

I have checked all the power up sequnces and they are correct. All the clock inputs to TPS65950 is correct

I can JTAG to DM3730 using blackhawk usb100v2 debugger, is there any register in DM3730 which can tell why it is not sending I2C command ?

Thanks,

Bhupesh