Team,
A strange catch diode heating issue is observed on one of our power boards. TPS5430MDDAREP as a buck converter to step down 12V to 3.3V in one of my designs. The catch diode used is B340A-13-F as recommended in the datasheet. The diode seems to get very hot when the device is turned on. The overall load on TPS is about 900mA. The temperature was observed using a thermal camera. Without any load connected, the diode is not heating up. Once we connect our other board, the diode starts heating. The diode starts heating even if we connect our second board with only 2 STM32 ICs (about 350mA).
Also there is another TPS5430 used on the same board to generate 5V from 12V. That seems perfectly fine.
D25 heating is the only issue. Rest works fine.