- i had used a design from webench and i am unable to get the output 20-32V__20V3.25A.pdf
i am attaching the schematic downloaded from webench which i used to generate the pcb the output from the board is 1.4v where i am giving input of upto 30v and my desired output is 20v from the pcb.
please help me with this
the observations are the en pin is high with 1.9v
the DR1H is showing 1.4v at resistor R3
the DR1L is showing 0.0V at resistor R4
i need 20v output at the vout.