Most of the IT enabled gas gauges in the TI line specify 1% capacity estimation accuracy once IT has run successfully. This spec is absent from the bq27541 literature. Is there any documentation on what capacity estimation and reporting accuracy I should expect when using the cell model for the Moli ICP1034503?