Other Parts Discussed in Thread: LM61480
Hi team,
The LM61480 PG threshold-falling in the Datasheet is set at 92%~96.5%, and the output voltage range is generally ±5%Vo (95%~105%), which means that it may occur when the output voltage is 95%~96.5%. PG flips. Generally, the PG signal of the primary power supply will be used as the EN signal of the secondary power supply. Is it unreasonable to set the upper limit of PG threshold-falling at 96.5%? The output voltage is still within the normal range. The PG flips and turns off. class? Or are there other considerations?