This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25184: Is SSR Possible, or Other Ways to Improve Regulation Accuracy?

Part Number: LM25184
Other Parts Discussed in Thread: LM25017

The datasheet states 1.5% accuracy.

I believe with output of ~ 4V, that's about 60 mV tolerance. 

I need to double or better the accuracy. Any way?

Also, can Vout be adjusted during operation?