Other Parts Discussed in Thread: BQ24230
Hi,
We manufactured a large number of PCBs using BQ24232, the battery included internal NTC, connected to the TS pin as shown in the picture. R12 not populated.
I tested the charging function with the same battery on 25 PCBs randomly taken from the batch. In some of them the LED is ON some of them the LED is OFF.
When the input is connected to the USB port CHRG LED blinks for a short burst which means the LEDs are OK and assembled on right orientation on the PCB
What can be the issue?
Thank you.