Part Number: BQ76905EVM
Other Parts Discussed in Thread: BQ76905
The customer is using BQ76905 to test the cell balancing function.
When TS mode is set 0; the cell balancing function is normal.
When TS mode is set 1; without 100kΩ to ground in TS pin, only 3 diodes to ground. the cell balancing function is normal.
When TS mode is set 1; with 100k to ground in TS pin, the cell balancing can not operate.
The customer need the 100kΩ.
Could you pls tell me why "When TS mode is set 1; with 100k to ground in TS pin, the cell balancing can not operate" ?
Whether this is the internal cell balancing algrithum?
Could you pls help to reproduce this in our EVM board?