Hi,
Can you please help answer the following question regarding the TPS65053:
When the switching converters are disabled, is there any sort of active pull down resistor?
The datasheet address the LDO's, but not the other outputs:
“If disabled, the outputs of the LDOs are pulled low by internal 350Ω resistors, actively discharging the output capacitor.”
Thanks,
Andrea Ramos