This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74401: One question about the datasheet

Part Number: TPS74401


Hello,

The datasheet writes "1% Accuracy Over Line, Load, and Temperature ", but I don't know what's the accurate meaning. Does it mean this chip's output voltage error related to the set output is less than 1% under all condition? Considered about that the max load regulation is about 0.9%, I don't think that's right.

Or does it mean the line regulation, the load regulation and the output error related to temp are under 1% respectively?

Thank you for your help.

Liu