This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, TI experts
The customer is currently reviewing the use of UCC27614 for N-channel MOSFET drive ON/OFF control
1.MCU GPIO -> TI UCC27614 -> N-channel FET Gate control must be performed.
First of all, if you press and hold the POWER OFF button on the product, the N-channel FET should be turned off, but if you look at the attached circuit diagram, it doesn't seem to be turned off accurately.
Q1) We request a review of the attached circuit for identification of any issues and suggestions for improvement.
Your assistance in assessing potential problems and providing recommendations would be greatly appreciated.
Q2) Is it possible to control ON/OFF of N-channel FET using UCC27614?
For reference, the function control configuration diagram is as follows.
[Function control diagram]
Please check. Thank you.
Hi Grady,
The UCC27614 will pull out to VDD when on, and pull to GND when off.
This setup essentially makes a voltage divider, where 4.7K is in parallel with R5 when a high signal is sent, and in parallel with R6 when the low signal is sent. This results in a gate voltage of 17.2V when high, and 11.4V when low. I simulated this and got the same result. By removing that voltage divider in simulation, the FET was able to be turned off.
However, the main problem (for Q2) is the source voltage. The FET is only on when Vgs is > Vth. UCC27614 is a low-side gate driver, intended to be used to drive a FET with a source referenced to GND. This is a high-side switch, and the UCC27614 does not have any level-shifting ability to adjust for the source voltage not being 0V.
Here are three options:
Thanks,
Alex M.
Hi, Alex
Thank you for reply.
Is there a device you can recommend as a high side switch?
Hi Grady,
Alex is currently OoO and will get back to you before end of this week.
Best,
Pratik
Hi Grady,
Sorry for the delay. I would direct your question to the team behind those products.
I can send this thread to that team.
Thanks,
Alex M.
Hi Grady,
What is the PWM frequency of this application? Our high side switches are not meant for PWM applications higher than 2kHz.
If f≤2kHz, we have the following single channel devices (linked) capable of handling 24V and 2.5A: options
Our new TPS281C100 could be a good fit. Please let me know if you have any questions about the device.
Best Regards,
Elizabeth