Other Parts Discussed in Thread: LM74500Q1EVM,
Hello,
I'm working on reverse polarity protection based on LM74500. This IC was chosen, because reverse current blocking is not necessary, so LM74700 is not needed.
Technical specs:
Vin_max=36 V
I_max=11 A
Used transistor is N-MOS PSMN4R1-60YLY, which has 60 V VDSmax., +-20 V VGSmax. and around 3.3 mOhm of RDSon at 15 V VGS.
Here is a schematic: 
I have few questions:
- on LM74500Q1EVM board, 33 V bidirectional TVS diode is used. Is there any reason that 36 V TVS diode is not used? I'm planning to use SMLJ36CA TVS diode, which has 58.1 V clamping voltage, which is lower than 60 V, so this diode should be still acceptable?
- is there any reason why 220 uF capacitor is used as output capacitor on EVM board? I'm planning to use 2.2 uF/100 V capacitor on the output and input side. Any concerns regarding this?
- is there any maximal value for Vcap capacitor that could be used? I'm planning to use 470 nF / 50 V capacitor, because the same capacitor type is already used for other purposes on the same circuit.
- do you suggest to use gate resistor to minimise peak gate current in to MOSFET transistor?
Many thanks,
Kind regards,
Dejan.