I'm checking out a new board which uses the TPS2493PW and ran into a couple issues. The input voltage is 54V and the current limit is set to 1.8A (0.028 ohm sense resistor). My output MOSFET is an IRF540NS. I am using a MOSFET (ZVN3310) to pull the UVEN low so I can disable the output when a switch is pressed acting as a reset.
If I power up without a load applied, the 2493 starts up. I can activate the reset and the output goes down. I can deactivate the reset and the output comes back. Once the power is up I can apply the 1.2A load and everything is well. I can then increase the load pass the 1.8A level and the 2493 shuts the output off. If I then back the load off to the 1.2A level the output comes back on. All this seems to work well.
Three issues so far:
1) If I apply the reset with the 1.2A load connected, the output goes down. This is what I expected. When I deactivate the reset (with the 1.2A load connected) the 2493 goes into fault. Each time the 2493 retries, it goes into fault.
2) If I apply the input supply voltage with the 1.2A load attached, I get the same result as in issue 1, the 2493 goes into fault and faults on each retry.
Would issues 1 and 2 be related to the power limiting? My PROG resistors are currently 100k and 15k.
3) If I bring the circuit up with out a load, the 2493 starts up as expected. If I then short the output, the 2493 goes into fault as expected, but when I remove the load, the 2493 does not retry.
I'm not sure why it doesn't retry, what should I check here?
Any inputs are appreciated.