This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: load

Part Number: BQ76952


Hello ti Expert!

Some Protections I might like to ask some protections when using bq76952. Now I need to use load removal to restore SCDL, and I want to use the host to control load on and off. So I have set the Protections:load Detect:Active Time to 0. Set Protections:load Detect:Retry Delay to 0 and Protections:load Detect:Timeout to 1. Then when I want to turn on load detection, I just need to use the command 0x009E while the device is running.

Looking forward to your reply.

thanks.