Other Parts Discussed in Thread: TXS0108E-Q1, TPS92201,
Hello, TI guys.
I am trying to design an IR LED driver circuit as below image.
Could you review and give me a feedback?
The condition is :
- Vin : 5V
- Ouput Current : 1A
- IR LED Vf : 2V
- PWM IO level : 1.8V
Q1.
The LED parallel structure is good to apply?
Q2. How about the inductor value?
Could you recommend any specific model?
Q3.
And also, I am worried about PWM IO level is OK with it.
The IO level from host IC side is fixed in 1.8V.
Should I use level translator to change IO level to 3.3V unless 1.8V is enough?
I use level translator(TXS0108E-Q1) for other circuit part and it have some spare pins.
Q4.
For PWM input, the right model is TPS92200D (1? or 2?) DDCR?
Regards