This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5810: Missing Package information for DSBGA-9 (YBH)

Part Number: LP5810

Hi,

I would like to use the new LP5810 LED driver in a new design, but I can't find any info on the TI site for the exact land pattern for the BGA variants. The site says it's a DSBGA-9 (YBH), but this package is not listed in the searchable list of packages, and the data sheet only has the land pattern for the WSON variants.

Is the DSBGA-9 (YBH) land pattern the same pitch and ball size as the other DSBGA variants with different pin counts? Those appear to all be 0.4mm pitch, ⌀0.2mm, although roughly half of the links to those documents are broken so it's difficult to get a high degree of confidence on that one. (side note.. someone from TI should go through the package list and fix all the broken links!).

Thanks in advance for any help,

Josh