Hi,
The PSpice for TI simulation model is used to verify the operation of TPSM33625. We created a 24V→5V Buck circuit and a 5V→-5V inversion circuit, but the simulation cannot be performed properly. Could you tell me where to change in the attached circuit diagram?
Overshoot occurs in the step-down circuit. Output is not possible in the reverse circuit.
I changed the condenser connected to the boot pin to a 1G ohm resistor and added a Zener diode to the output stage of the inversion circuit, but it didn't work well. I wanted the boot pin to be Non-connect, but I couldn't run the simulation, so I connected the resistor.
Best Regards,
Nishie