This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: How to delay transmitting sink capabilities to a source until needed

Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65988,

Hello, I am utilizing the TPS65987D as a sink that is attached to charging ports via CC lines (my source which is a TPS65988) for testing. I am looking for a way to program the TPS65987D using the TI Application Customization tool such that the sink does not attached to my source upon power up but rather begins unattached from the sources perspective until I request it to transmit its sink capabilities at a later time. More specifically I need the Type C State Register of my source to read as an unattached source. Is there is way to achieve this through the firmware generated by the TI Application customization tool, or by altering the configuration on ADCIN1 while the source and sink remain physically connected on the CC lines?

Thank you,

Eoin