Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5069: Output oscillations

Part Number: LM5069

Hello,

I have a design with two LM5069 placed back-to-back to act as a bidirectional switch and both switches are closed during my tests. There is an AC/DC stabilized power supply (54V) on one side and a 10S-3P battery charger on the other side (Linear Tech. LTC4020). Signal OUT_SWITCH and EL_LEFT_MES were measured and are identical.

I believe both the charger and the AC/DC induce a bit of ripple on the power line.

At specific charging current, the transistor of the LM5069 on the AC/DC side is acting linearly and overheats, leading to the transistor destruction and the output is oscillating (see below).

I checked the fault timer pin and it doesn’t rise, meaning this is not linked to the power limit or current limit.

I bypassed the OVLO protection and the problem persists and there is no UVLO protection in my design.

I checked the GATE pin. When acting normally, it is 12V above VIN as stated in the datasheet. When the output starts to oscillate, it drops to about 3V/4V above VIN (see below).

I added a capacitor between the transistor drain and ground and it improves the switch behavior without fully correcting it : the output doesn’t oscillate as much but V(gate) is still not stable for a while (see below).

  

Did you already encounter a similar issue with this component?

Any idea what could be the reason of the oscillations?

Thank you,

Best Regards.

  • Hi Clément,

    Welcome to E2E !!!

    May I know at what current level this oscillation is observed? 

    How is this current measured? Scale is showing as 50 mV/div.

    Proposal-1: Place 10Ω resistance at R1004 and 10nF ceramic capacitor at R1011. Please see the performance.

    Proposal-2: Remove this below circuit. Please see the performance.

                       

    Proposal-3: Remove Q1000 and connect the OUT_SWITCH net directly to EL_LEFT_MES. Please see the performance.

  • Hi Avishek,

    Thank you for your reply!

    The current was measured with a current clamp. The screenshot actually shows a measure of the AC/DC output current with a 1A/V scale. The charging current on the LTC4020 side is a ramp-up of 50mA/step. The oscillations happen at a charging current of 200/250mA.

    Thank you very much for your proposals. I will try them all and get back to you with my results.

    Best Regards,

    Clément