Other Parts Discussed in Thread: UCC28951, PMP8740
Hi,
I have designed a 20V output power supply using UCC28951. It is successful. The DEMO I am referring to is TIDA-020031.
While I need to design a 70V output power supply. The current is 45A and power is 3000W. Can I use UCC28951 to implement it?If possible, what are the advantages and disadvantages? Is there a suitable DEMO reference available?
At the same time, I would like to inquire about the difference between a center-tap SR and full-bridge SR for 70V output. Which method is more suitable for my design?
Thank you very much!