Other Parts Discussed in Thread: TPS2640,
1. During a surge test, EFUSE was damaged when -3kV was applied to line to line or when -4kV from N to PE is applied, Efuse is damaged.
Waveform explanation below) CH1 is the EFuse input voltage, CH2 is the EFuse output voltage, and M is the voltage of CH1-CH2.
Related circuit)
If you proceed with various countermeasures, for reference, check the surge countermeasure data for TPS2640 to add a TVS diode to the input/output terminal, and no EFuse damage occurred during surge evaluation. However, if TVS was added, Efuse damage occurred for some reason when a surge was applied. I don't understand how it was prevented, so please explain.
<TPS2640Notes>
---EFUSE input/output terminal voltage when surge is applied after adding TVS---
Inquiry details
1. EFuse damage mechanism when surge is applied
2. Mechanism that prevents EFuse from being damaged when surge is applied when adding TVS on top of EFuse after damage.
3. Why is the TVS missing from the input/output terminal of the TPS26601 when a surge is applied? Is this an unnecessary part? I know you are busy, but please reply.