Hi
We have occur OCP issue, TPS55288 INT pull low when connect 5V/3A device, we are checking for output current.
Please help check if below schematic have any need modify.


Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
We have occur OCP issue, TPS55288 INT pull low when connect 5V/3A device, we are checking for output current.
Please help check if below schematic have any need modify.


Thanks!
Jeff
Hi Jeff,
May I know what is the customer and the application here? And what is the input voltage, output voltage and output current?
Please notice that when SCP/OCP/OVP bit is set, then INT pin will output low. Please probe SW1, SW2, Vout and the inductor current waveform to see if any protection is triggered.

BRs,
Bryce
Hi Jeff,
It is recommended to add the resistors and filter capacitor between ISP and ISN pins, so the output current sense could be more precise. What about the current limit at Buck mode?

And also considering the spec of ISP-ISN current limit voltage has variation, it is better to leave some margin for output current protection threshold.

What is the max output of TPS55288? 20V/3A for 60W? Mulin will share more comments about the schematic and layout.
BRs,
Bryce
Hi Jeff,
Below is my feedback about schematic:
1.Recommend to change R79 and R80 to 0ohm.
2.Remember to connect SCL and SDA pin to VCC with 2.2kohm resistor.
3.Add RC filter as Bryce suggest.
4.Recommend to add several ceramic capacitors in the Vout pin (for example, 10uF*3 as EVM). This can reduce output voltage ripple and can increase output current accuracy.
5.Recommend to add a 0402 0.1uF ceramic capacitor in Vout pin and put it as close as to the chip.
About the layout, please see the attached file.TPS55288 layout reiview 20240116.pptx
Regards,
Mulin