In the description of the Input Interlock Protection (8.3.7) are we to assume that using a resistor between DLH and ground, of some value between 100k and 220k, somehow sets the universal deadtime for the device when using the device in independent mode? The text in this paragraph, "There is no fixed time deglitching for this feature [interlock protection] in order to not impact the propagation delay and dead time of the driver." leads me to believe the resistor on the DLH pin somehow still controls the dead time for the device. Can someone expand on this description?
Thanks,
Mark