Other Parts Discussed in Thread: LM5149, LM5116, PMP7282, PMP, LMG5200
Hi there!
For an input voltage range of 36–60V and an output value of 14V, 70A, I am designing a DC converter (Synchronous Buck). Operation of CCCV is necessary because it is used for battery charging. The LM5148 & LN5149 IC is what I found because there isn't a specific ASIC for this requirement. Therefore, I would like to change the design to meet my needs. Please let me know.
1) Is there CCCV support for LM5148/LM5149?
2) Considering its lower current capacity, is it possible to synchronize two ICs (converters) for dual phase operation, similar to what PMP7282 for LM5116 does?
3) In an effort to enhance the design, we were considering using GAN FETs. Can we and how can we do this?
4) In terms of size, thermal capacity, and current, what would the benefits of employing GAN be?
Thank You.