Other Parts Discussed in Thread: EV2400, BQ40Z80, GPCCHEM
Equipment:
- BQ40Z80EVM-020
- Rechargeable Lithium Ion Battery Model : INR18650HJ2 (4 units)
- laboratory power supply
Jumpers position:
| J3 | J4 | J5 | J6 | J7 | J8 | J9 | J10 | J13 | J14 | J15 | J16 | J17 | J18 | J20 | J21 | J22 |
| None | None | PIN12_PRES | PIN15_VC7EN | PIN12_VC7SNS | None | None | PIN16_CB7EN | None | PIN13_LED | PIN20_LED | PIN22_LED | PIN21_LED | EV2400_SMBD1 | PIN12_onward | PIN13_onward | EV2400_SMBC1 |
Tried to achieve a successful learning cycle using the following official guide: https://www.tij.co.jp/jp/lit/an/slua903/slua903.pdf?ts=1705308902556&ref_url=https%253A%252F%252Fwww.google.com%252F
After completing the guide re-action and even additional cycles, the "Update Status" field in memory is still 0x04, but the guide should be 0x05 and then 0x06.
List of parameters changed before the start of the learning cycle:
| Parameter name | Value |
| Enabled Protections D | 0x0F |
| DA Configuration | 0x10 |
| Cell Configuration | 0x04 |
| Protections/COV | 3900 |
| Charge Term Taper Current | 50 |
| Design Capacity (mAh) | 3000 |
| Design Capacity (cWh) | 4320 |
| Voltage Threshold | 2500-2600 |
| Qmax | 3000 |
| Term Voltage | 10000 |
Why doesn't "Update Status" change its value? How to fix it? Are there any other ways to ensure a successful learning cycle?