Hi BU expert,
Can the no-load and loaded status of TPS2546 be judged by the high and low levels of PIN 9 STATUS? When TPS2546 is no-load, PIN 9 is high level, and when TPS2546 is discharging, PIN 9 is low level, right?
Are DM_IN and DM_OUT connected when TPS2546 is powered on? Are DP_IN and DP_OUT directly connected?
If the power is not turned on, then DM_IN and DM_OUT are not connected? DP_IN and DP_OUT are not connected?
Regards,
Charlie