Other Parts Discussed in Thread: BQ78350-R1A, , MSP430FR6989
Hi,
I am considering to use the BQ76930 cell battery monitor for a configuration of parallel cells, I want to use it with the BQ78350-R1A to form a complete BMS.
I would like to know if it is possible to connect several BMS (built with the previous components plus a companion controller) in parallel to control each combination of packs which are going to be connected in parallel. I attach an image to be more comprehensive.
I don't want to use only one BMS for all the structure because it would require to connect all the internal points of the series cells, so for that reason my question is more related to use several BMS in parallel, with the intention that each BMS controls only a branch.
Do you consider that is needed to add a blocking diode to protect each pack?
Thanks in advance.