This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: BQ40Z50-R2 calibration usage

Part Number: BQ40Z50-R2

Hi 

    There 3 series connection module designed by using BQ40Z50-R2, and the product had been done the calibration by the cycles of full charge and full discharge , a question need to confirm that if it has to do the same process of full charge and full discharge in customer ,or just only requires 10% or 20% ...charge and discharge is ok ? because the calibration time is too long to customer if finish the completed process.  thanks so much ,pls advise .

  • Hello,

    If the learning cycle has been successfully completed for the gauge, there is no need for the customer to repeat it. The purpose of the learning cycle is for the gauge to create the Ra table and Qmax values, so once they are created the customer should be able to use them through uploading the .srec file.

    Regards,

    Anthony Baldino