This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Questions About R2 version 2.02.31 and all 34z100 Device

Part Number: BQ34Z100-R2
Other Parts Discussed in Thread: GPCCHEM

Hİ,

-I read the release note about the R2 revisions but ı can't understand how you increased the current rate and capacity rate because we already use currscale for capacity above 29Ah capacity and above 32768mA current rate, and these registers have a maximum value of 255 at G1 version and its same in R2 version if these values are same what makes the difference for the "a newer version of this product is avaible" note for "Supports larger size battery applications " or you suggest another way for increase a capacity and current rate.

-If we need to use currscale we need to use capacity scale( or not, If you think differently please tell me)  but its not clear for me are we need to use energy scale too, because we don't use the energery parameter but if it affects the SOC we can configure.

-Do you suggest using a multicell and high capacity application for R2 2.02.31 or G1 version

Best regards,