This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61094: will it do vin = 5v to vout = 3.3v?

Part Number: TPS61094
Other Parts Discussed in Thread: TPS631000, TPS63901, TPS63900

i read this from some time ago (locked now, see linked thread):

Hi Jhon,

If VIN >= VOUT, the device works in pass-through or by-pass mode, no matter which mode the device is, the VOUT is close VIN, not the target voltage you set.

TPS61094 is a buck / boost device, it means it can work in boost mode (VIN to VOUT) OR buck mode (VOUT to SUP when charging).

I think what you need is buck-boost device (please be noted that buck / boost differs from buck-boost), like TPS63901 or TPS631000.

Regards, Nathan

the tps61094 datasheet does however have this example (5v to 3.3v)?? seems exactly the other way around? Vin > Vout, Vin buck to Vout

i need more or less what is in this figure 8-14. will it work? or do i need another part?

thanks

frank

  • Hi Frank,

    When VIN > VOUT, vin doesn't buck to VOUT, VOUT follows VIN. The 'Buck' means that VIN will buck to SUP to charging supercap, not buck to VOUT.

    When VIN < VOUT, SUP will boost to VOUT to the target output voltage you set.

    So what is your requirement? Seems that TPS61094 is not a good option for you.

    Regards,

    Nathan

  • hi nathan,

    how about the example in the datasheet? it shows 5v in and 3.3v out??

    is there another ic that can do this?

    my requirements:

    - 5v in, max 250ma

    - 3.3v out, average 150ma

    - large cap to supplement large current spikes on 3.3v application

    thanks

    frank

  • Hi Frank,

    The 3.3V in d/s here actually means that it can support 3.3V in charging mode, not buck mode. Maybe there is a little confused here... TPS61094 can only support 3.3V in charging mode, but in buck mode, the VOUT follows VIN, can't be a stable 3.3V.

    Sorry we don't have a integrated IC that can meet you requirements. Maybe you can consider a separated solution, by using a Buck IC (for 5V to 3.3V)  + Boost IC (for cap to 3.3V) + charging IC (or LDO, for charging the large cap).

    Regards,

    Nathan

  • how about the TPS63900?

    that seems to do the trick?

    thanks

    frank

  • Hi Frank,

    TPS63900 can work for 5V to 3.3V and cap to 3.3V, but it can't charging the super cap, you still need a charger IC or a separated charger circuit.

    Regards,

    Nathan