Other Parts Discussed in Thread: BQ24075
Hi,
I am currently using BQ24075-Q1 in my design to charge a 4.2V Li-Ion battery from an input 5VCC so that when the input is not available I can drive my load from the battery.
My load is an MCU that needs 1.5V and 3.3V as well as a 5VCC to run. So when the 5VCC is not available I have to generate these supplies from my battery voltage to run the MCU.
Is there a PMIC that can charge my battery and at the same time has an internal buck boos converters with multiple outputs that can generate 5V, 3.3V and 1.5V for me from the battery voltage when the internal 5VCC supply is not available? If not is there a PMIC I can use along with BQ24075 that can buck-boost my battery voltage (max 4.2V to min 3V) to generate 5V, 3.3V and 1.5V supplies,
Please let me know,
Thanks