Hi Expert
How can I understand the IIH,EN?
The max value of REN is 500KΩ. Then the input current will be 5V/500KΩ=10uA which is less than 14uA. The EN pin maybe not be drived.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert
How can I understand the IIH,EN?
The max value of REN is 500KΩ. Then the input current will be 5V/500KΩ=10uA which is less than 14uA. The EN pin maybe not be drived.

Hi Song,
This is just the typical current that is pulled into the IN pin during VIN=5V. The device is not a BJT style device that requires a BASE current to operate.
Please note that we do not spec a min or max and this is only to take into account the scenario of driving many inputs from one GPIO/MCU output.
Thanks,
Shreyas
Hi Shreyas
Thanks for you answer!
What is the max resistance that can be added in series of EN drive line?
Hi Song,
For this device, we recommend using a 5kOhm protection resistance.
Thanks,
Shreyas