This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76942: OTP programming bq76942

Part Number: BQ76942
Other Parts Discussed in Thread: BQSTUDIO

We have fabricated and assembled the two layer test board avaiable on TI website for 7 cell BMS(3.7V*7=25.9V battery).

Using the bqstudio and BQ76942EVM we are able to communicate with the 2 layer board device using jumpers.

Pls help us generate the OTP image file for the device on 2layer test board to work in standalone mode (without processor).

Below is our specs:-

1.) Over voltage protection:30V(4.28V per cell)

2.) Under Voltage protection:19.8V(2.82V per cell)

3.) Operating temp range:- -30 C to +55C

Kindly share the OTP file which we can directly burn in the OTP on the test board available on TI website so that the above specs are met, when device boots in standlaone mode.

Or atleast share the configuration file generation steps.