Other Parts Discussed in Thread: TPS23731EVM-095, TPS23731, TPS23734EVM-094, TPS23734, TIDA-00617, TPS23751, TPS23751EVM-104, TPS23754, TPS23861, TPS23861EVM-612
Hello, I'm looking for selecting the PD(Powered Device) IC, type2 class4(max 25.5W) which complies IEEE802.3at
Are there any PD IC which contains DC/DC converting function exist?(No need for peripheral neither flying back converter nor general DC/DC converter)
If there are then please recommend me the PD IC.
We want to convert 48V -> 5V.(input/output power 25.5W max)
We are looking for class 4 so that we need the circuit which guarantee the input and output power of PD IC for 25.5W(assume the efficiency as 100% for easy calculation), Hope we find the right one.
Thank you.
Sincerely Yours,
Subin Ko.