Other Parts Discussed in Thread: TUSB320, TPS65987D, TPS65987
I am currently testing the TUSB320.EVM. We require DFP, UFP, DRP and to be able to swap Sink and Source positions. Specific to our case we are trying to achieve Source at the UFP position and Sink at the DFP position to be able to charge 5V 3A to the host portable devices such as a personal tab or iPhone. I am not sure if the TUSB320 is the correct PD controller for this purpose. However this is one of the only PDK's that are available. Any assistance would be greatly appreciated.
Regards,
Don Carmichael
Radial Engineering Ltd
donc@radialeng.com