Hi,
I'm trying to design with the LM5146-Q1 an output of 0.85V and 20A from a input voltage range of 8V to 36V (it has to withstand spikes voltages of 100V too).
From Webench and from the excel file I've got very high power dissipation from the MOSFETs.
I wanted to ask if it is possible to have two LM5146-Q1 in parallel to distribute the power dissipation. If yes, is there a reference design I could use?
Thank you,
Jorge Cruz