This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5156: LM5156: LM5156/55 output fluctuation with no load

Part Number: LM5156
Other Parts Discussed in Thread: LM5155,

   1385.LM5155_56_Excel_Quickstart_Calculator_for_Flyback_Regulator_Design.xlsx

I have designed a DC to DC flyback converter using LM5156. The schematic and regulator design files are attached. I am getting abnormal behaviour. With no load its saw tooth wave over the output giving voltage fluctuation from 5v to 15v. After putting the load more than 8W it becomes stable. As the load is less than 8W it behaves like capacitor charging discharging. By decreasing the output capacitance from 1mF to 500uF the ripple is less for less power (e-g. It works fine after 5W with less output capacitance).

The problem as load takes less power on start up. It fluctuate and the load is not starting up. Please suggest on how it can be fixed. Ideally it should be stable with no load. Is it linked with soft start-up. SS or. Please suggest any solutions.

Thanks.