HI team,
If no need for OVP UVP how to set it? thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
You can connect UVLO pin to input voltage to remove UVP function. Do not leave it floating.
(datasheet pg 18, section 9.3.1)
For OVP function, let me check on how to disable that function.
Best Regards,
Arush
Jimmy,
Do you wish to disable the OVP feature or are your application doesn't require the feature. If your application is below 33V then you can connect OVP pin with RTN which will use default OVP of 33V. Can you confirm this once?
Best Regards,
Arush
Hi team,
Customers do not need OV UV function.
So I just let UV pin to Vin and OV pin to RTN. That all. right?
Jimmy,
OV pin to RTN will give you OVP of around 33V. Is customer fine with this?
Best Regards,
Arush
Hi team,
OV pin to RTN will OVP around 33V.
If UV pin to RTN. What voltage of the detect point?
Hello Jimmy,
If the UV pin connected to RTN, the device will use default voltage as detect point. These default values are 14.9V for rising and 13.8 for falling.

Best Regards,
Arush
Hi Team,
But you told me if no need for UV just contact Vin. I want to ask even Vin down to zero never trigger UV. Is right?
Hi Jimmy,
We can disable UV. Either you choose default UV or configurable UV.
Regards
Kunal Goel