Part Number: LM46002
Other Parts Discussed in Thread: LM46001, LMR43620, LMR33620
Team,
do we have efficiency data for this device when using 2MHz switching frequency?
Here's my customers spec:
- Vin = 8..32V
- Vout = 5V
- Iout = 1mA..500mA, but in failure cases up to 1.5A
They had planned with the 1A version (LM46001), but due to the failure case probably need to go to th 2A version.
Questions
- Is it possible to use both devices with these specs at 2MHz?
- I see that switching f decreases in light load condition
- Is there a minimum current for the regulation to still work?
- Anything else that needs to be considered?
Best regards