This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2825: Max Duty Cycle

Part Number: UC2825

From the datasheets it can be seen that the maximum duty cycle for this part is 80%

I work in voltage mode, open loop  and cant achieve more than 50% D.C. 

Does the controller really have the ability to work at 80%?

please your advise 

  • Idan,

    How are you determining the max duty cycle to be less than 50% - are you looking at OUTA or OUTB only? of, OUTA is limited to ~40% and OUTB is also limited to ~40% but when you consider the total duty cycle of both outputs you get 80% max. Duty cycle definition for a dual output PWM is defined this way.

    Regards,

    Steve

  • Thank you for your answer.

    Each output of the controller is connected to a power MOSFET through a driver.

    I'm looking for a controller that can supply 80% or above thus creating an overlap between the outputs

    Can you recommend TI part that can be suitable?

    Regard,

    Idan

  • Idan,

    Your application sounds unique in that it is not regulating output voltage of a switching power converter. I don't know of an analog PWM operating the way you describe. I found some examples of similar E2E threads asking about overlapping PWM signals. In almost all cases the control for this is coming from a microcontroller (MSP430). You might try submitting a new E2E thread targeting the microcontroller team support by mentioning MSP430?

    Regards,

    Steve