This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Requirement of negative input to negative output buck converter

Hi TI team,

I have a requirement of negative input voltage to negative output converter.

Input voltage:- -22V to -27V

Required output voltage:- -5V or -3.3V

Also, suggest another converter with negative input voltage and positive output voltage.

Input voltage:- -22V to -27V

Output voltage :- 5V or 3.3V(For microcontroller)

Thanks & Regards,

Prakash