Hello,
I was hoping if TI could help me recommend a battery fuel gauge or an IC that would protect our batteries at cut off when they are depleted. We are using Mil-Spec batteries, particularly the rechargeable BB-2590 and BA-5390. We have a hysteresis circuit that cuts of the supply from the battery at 10V and won't turn back on until it sees 10.5V. Our customer gave us a heads up that during testing with the batteries mentioned above, they saw their units continuously turning on and off at the cut off voltage on another application. They did not give us a measurement as to how high the deplete battery voltage level went up other than saying that it turned on and turned back off. For safety reasons, we would like to make sure that if a battery has been deplete that it does not go thru this cycle.
My questions for the TI team is:
- Are there any fuel gauges that would be recommended to monitor the batteries mentioned?
- Should the hysteresis circuit account for a much higher voltage level for it to turn on? Since we don't have values, we are not sure that the depleted batteries will jump, say, from 10V at depleted state to 12 V with no load and then back to 10 V with load.
Any help would be appreciated. Thanks in advance.