Part Number: TL431LI-Q1
I would like to ask the maximum off-state current of TL431LI-Q1 at 125°C.
There are contradictory information in the datasheet. I use the following datasheet:
https://www.ti.com/lit/ds/symlink/tl431li-q1.pdf
There is a table item in 7.5 (Off-state cathode current )
![]()
which says that the off-state cathode current is in the range 0.1...1 uA, where 0.1 uA is the typical value.
However, according to the following figure (figure 4 in the above datasheet), the off-state current at 25°C is approximately 0.001 uA (or probably less, it is around zero).

The two typical values (0.1 uA in the table 7.5 and the value 0.001 uA in Fig 4) are very far from each other. Figure 4 shows that the off-state current is 0.008 uA at 125°C but because the current at 25°C is very far from the typical value, I don't know how to extrapolate for a reliable but realistic worst-case upper bound.
Do you have some measurement or other reliable estimation for 125°C (or similar temperature range) for the off-state current?