hi Friend,
I want to know the sleep mode efficiency of LMR43610-Q1 and quiescent dissipation . thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi Friend,
I want to know the sleep mode efficiency of LMR43610-Q1 and quiescent dissipation . thanks
Hello
When you say "sleep mode", do you mean shutdown mode or when the regulator is
providing an output voltage ?
What input voltage, output voltage, load current and inductor are you interested in ?
Are you using the device in ADJ mode or fixed Vout mode ?
Are you using the device in Auto mode or FPWM mode ?
Thanks
hi Sir,
In the low power mode, my understanding is that when IC enters the automatic mode, the efficiency should be higher than that when IC enters the FPWM mode, so I would like to ask you, and please tell me the efficiency of the low power mode under the two modes, sleep mode and FPWM mode. Please note that my operating conditions are input 9-18V and output voltage 3.3V.
Hello
The efficiency for your case can be found in the data sheet in the "Application Curve section".
Thanks