Hi
The customer design with BQ77915.
After the battery output load is short-circuited, remove the short circuit immediately. The CHG and DSG are always low. Only when the charger is connected, the CHG and DSG pins return to high.
In addition, if they are left without any load, after a long time BQ7791514 will enter sleep. Only when the charger CHG is connected, DSG will return to the high.
Attached the schematic.

Please help check it.
Thanks
Star