Part Number: UC2525A
Other Parts Discussed in Thread: UC2525B
Dear sir,
Quick questions to UC2525:
Q1: What about the difference between UC2525A and UC2525B?
Q2: any other new device to update UC2525 family?
Regards,
Jack
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jack,
Thank you for the question! This table highlights the differences between the A and B versions in detail. Regarding your second question, we do not recommend new systems using the UCx52x family. The TL494 controller can be implemented in place for the UC2525A/B for new designs, but any existing systems would need a redesign as it is not pin to pin with the UC2525A. It is a versatile controller to be used in a variety of applications and will be supported well into the future in our 300mm factories.
Best,
Andrew