This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63603: Can a 1K pull-up to 5 volts be used to power an LED on the PG pin

Part Number: TPSM63603


The datasheet mentions that the PG pin as "The typical range of pull-up resistance is 10 kΩ to 100 kΩ"  I was wondering if a 1K pull-up to 5 volts can be used on the PG to power an LED?