Hi Expert.
I would like to apply a new function that allows the user to limit the charging amount while using the battery pack.
Which concept is user select the DOD 80% or 100% (Depth Of Discharge) for battery safety and SOH.
I have plan to change the following registers via 0x44 write command,
I'm worried about SOC accuracy because there is no running cycle.
Is there anything worth mentioning?
1. FD : Set Voltage Thd. Clear Voltage Thd
2. TD : Set Voltage Thd. Clear Voltage Thd
3. Term Min Cell V
4. Design Capacity (mAh) , Design Capacity (cWh)
5. FC : Set Voltage Thd. Clear Voltage Thd
6. TC : Set Voltage Thd. Clear Voltage Thd
7. Charge Voltage : all temp. range
8. Protection Thd.